Cooling water directly from the Baltic Sea
Turbidity measurement with the CUS52D plastic version
The Rostock power plant uses cooling water from the Baltic Sea and pumps it back into the sea after use in order to maintain the water cycle. A turbidity measurement must take place with the required supporting documentation to protect the environment and ensure that the water returned to the cycle does not contain any impurities.
![Baltic Sea water used as cooling water in the power station Baltic Sea water used as cooling water in the power station](/__image/a/9302807/k/8144052410a8f1493e418adad7cd8fda14e46c75/ar/2-1/w/1024/t/jpg/b/ffffff/fn/KNG_Kraftwerk.jpg)
KNG benefits with the Endress+Hauser solution from
Highly accurate measurements.
Reduced maintenance costs.
High availability.
-
Compliance with turbidity limit values and as documentary proof of the parameter for supervisory authorities.
Customer challenge
The power plant draws cooling water from the Baltic Sea and uses it almost untreated. It is pumped back into the Baltic sea after it has been used as cooling water. This process is monitored by means of the turbidity measurement as this parameter can be used to detect possible impurities and thus identify leaks in the cooling water cycle.
Our solution
The high salt concentration of the Baltic Sea water creates a very harsh environment for the material and regular maintenance. The plastic version of the new CUS52D turbidity sensor is used in order to increase the operating times of the turbidity sensor and prevent possible breakdowns due to corrosion. The resilient plastic of this sensor prevents material changes and any functional restrictions. The plastic sensor measures reliably even at low turbidity values.
Turbidity sensor CUS52D-AA1HA3
Transmitter Liquiline CM442-AAM2A2F210AA 2
-
Standardprodukter
- Pålitliga, robusta och lätta att underhålla
Tekniska egenskaper
Enkelhet
-
Specialprodukter
- Designade för krävande applikationer
Tekniska egenskaper
Enkelhet
Varierande
FLEX urvalet | Tekniska egenskaper | Enkelhet |
---|---|---|
Fundamental urvalet Möt dina grundläggande mätbehov |
Tekniska egenskaper
|
Enkelhet
|
Lean urvalet Hantera dina kärnprocesser med enkelhet |
Tekniska egenskaper
|
Enkelhet
|
Extended urvalet Optimera dina processer med innovativa teknologier |
Tekniska egenskaper
|
Enkelhet
|
Xpert urvalet Hantera dina mest utmanande applikationer |
Tekniska egenskaper
|
Enkelhet
Varierande |